Energy chains
Bikes instead of cars: for the mobility transition to work, cities need more parking facilities without encroaching too much impact on the cityscape. For this purpose, the Japanese manufacturer Giken has built a garage called Eco Cycle, which parks bicycles completely automatically underground. To ensure the reliability of the robot garage, the engineers used robust and maintenance-free energy chains from igus for the lift’s cable guidance system.
The champagne corks are popping in Portugal, more precisely at the Institute of Astrophysics and Space Sciences at the University of Lisbon. The researchers won the golden vector award 2024 for their MOONS spectrograph. Every two years, igus honours the most spectacular energy chain applications with this award – this year among 328 entries from 37 countries. The silver vector goes to the company TDK RF Solutions, which has developed a test rig for driver assistance systems, the bronze vector to MECAoctet for their movable nightclub ceiling. Bear Machines GmbH was delighted to receive the green vector for particularly sustainable energy chain applications for a machine that automatically recuts tyres.
For cable guidance in drawers and pull-outs of all kinds, igus is launching the draw e-chain. Thanks to the minimalist design, the price of the compact energy chain is 30 per cent lower than the most cost-effective standard e-chains. This protects against expensive oversizing, especially if the application is only moved a little.
If machines or systems are at a standstill, this costs production companies valuable time and money. To make it easier for customers to install energy supply systems and reduce installation time, igus offers the readychain service with pre-assembled systems consisting of chain, cables, connector and many other components. What makes it special: igus offers customers everything from a single source igus. The energy chain is filled, fully harnessed with connectors, quality-checked and delivered ready for connection – on request in the exact installation position. igus is now supplementing this service with a new “assembly helper”: the fast positioner. This simple tool makes handling ready-to-install e-chains even easier.
igus has added an ESD variant specifically for highly sensitive cleanrooms to its e-skin flat series. The modular ribbon cable’s new material prevents the chain from becoming electrostatically charged while ensuring that it generates no particles, even during very fast movements. The modular design with individual pods also allows quick energy supply system filling.
New addition to the igus energy chain portfolio: the E4Q, a globally proven e-chain for applications with large unsupported lengths and high fill weight, now has a new variant: the “L”. Users for whom the E4Q is too large can now save costs of up to 20% with the E4Q.64L. They will still benefit from the advantages of its big brother, such as quick, tool-free opening.
In production, downtimes are expensive. For manufacturers of such items as machine tools, it is therefore very important for system assembly work to be as quick and efficient as possible. The readychain rack is a modular assembly and transport rack for harnessed energy supply systems, one that igus has been offering for ten years. Now, igus has developed a solution that is even simpler and faster, with practically unlimited customisation potential: the first 3D-printed readychain p-rack (printed rack). It can be adapted to customer requirements with millimetre precision.
Things don’t have to be expensive. This is true not only of groceries, but also of energy chains. The simplest products often not only cost the least, but also represent the best technology. igus has now developed the snapchain 2.0 especially for low-stress and flat cable packages. The energy supply system consists of just one side link, to which cables can be fixed with cable tiewraps. It is made entirely of recyclate, so it is a sustainable solution.
Whenever the highest hygiene standards are required, igus scores high with lubrication-free and abrasion-resistant plastic components for movement. In particular, battery production for tomorrow’s mobility requires special environmental conditions, which are achieved through the combination of dry rooms and cleanrooms. The Fraunhofer IPA has developed a new type of certificate for precisely these requirements. The E6.29 energy chain from igus is the very first cable guide system that has been tested under dry cleanroom conditions and has now been certified with ISO Class 4.
In applications with loads of more than 80Mpa, plain bearings made of thermoplastic materials can be pushing their limits. igus has expanded the existing range of standard plain bearings with the new igutex fibre wound plain bearing series. The series displays its strength in heavy-duty areas such as construction machinery or hoists. The latest development in the product family is the material igutex TX3. It offers an even higher running performance with high dynamic forces than previous igutex bearings.