The starting signal has been given, the igus:bike® is on a world tour. To celebrate igus’s 60th birthday, the innovative, bright orange bicycle made from recycled plastic will be travelling the world for a whole year. The aim: to familiarise industry partners, media representatives and consumers with a new form of urban mobility that combines a fun ride with sustainability. The urban bike represents many of the advantages of igus products, the “motion plastics”: it does not rust, requires no oil and is virtually maintenance-free. The ball bearings, drive and freewheel also do not need lubricating as they are made from high-performance plastics. At the same time, the igus:bike is an example of how the transformation to a sustainable circular economy of plastics can succeed.
Whenever the highest hygiene standards are required, igus scores high with lubrication-free and abrasion-resistant plastic components for movement. In particular, battery production for tomorrow’s mobility requires special environmental conditions, which are achieved through the combination of dry rooms and cleanrooms. The Fraunhofer IPA has developed a new type of certificate for precisely these requirements. The E6.29 energy chain from igus is the very first cable guide system that has been tested under dry cleanroom conditions and has now been certified with ISO Class 4.
A low-cost robot operated via a VR headset. Spare parts identified and ordered in seconds using AI on a smartphone. A mobile app that immediately identifies potential applications for lubrication-free parts on an excavator. igus launches a selection of digital tools in 2023, as well as products and services which are easy to use and reduce cost. The goal: provide easy access to the right motion plastics product and have fun on the way, while being carbon-neutral and without plastic waste.