With the igus Mobile Shore Power Outlet (iMSPO), igus has developed a mobile connection system for shore power supply that can be positioned at any location along the terminal where a ship is berthed. This solution, which is already in use at the Port of Hamburg, received the “Ports and Harbor Innovation of the Year” award at the Electric & Hybrid Marine Expo Europe 2024 in Amsterdam.
The German economy is weakening and will only recover slowly in 2024, according to the Institute for Macroeconomics and Business Cycle Research (IMK). The mechanical engineering industry is also feeling the effects. To strengthen competitiveness, organisations will have to focus on automation. Thanks to Low Cost Automation (LCA) and the RBTX robotics marketplace from igus, companies of all sizes can find a complete solution that suits their requirements and budget – from as little as €2,000. The plastics company is now honouring the projects with the fastest return on investment (ROI) with the ROIBOT Award for the third time. Users can now apply to win LCA products worth €5,000 in addition to international recognition.
With the new chainflex cable CF33.UL, igus has developed the world’s first motor cable for energy chains and cable trays with UL approval and a four-year functional guarantee in the energy chain. This allows the cable to be laid seamlessly from the energy chain to the cable tray without a plug connection in between. The CF33.UL also adds a shielded PVC motor cable to the chainflex range.