With the igus Mobile Shore Power Outlet (iMSPO), igus has developed a mobile connection system for shore power supply that can be positioned at any location along the terminal where a ship is berthed. This solution, which is already in use at the Port of Hamburg, received the “Ports and Harbor Innovation of the Year” award at the Electric & Hybrid Marine Expo Europe 2024 in Amsterdam.
3D-printed polymer components will be able to resist much higher temperatures in future – in the engine compartment of a car, for example. While commercially available SLS printing materials threaten to deform at over 80°C, the new powdery material iglidur i230 from igus can withstand a long-term application temperature of 110°C. Furthermore, it is free of PTFE and around 80% more wear-resistant than the classic PA12.
Cologne/Hanover, 21st February 2024 – To support industrial companies with the challenges of our time, such as the transformation to Industry 4.0 and CO2-neutral production, Cologne-based motion plastics specialist igus is relying on triple intelligence at the Hannover Messe: artificial intelligence, plastics intelligence and Cologne intelligence. The exhibits include smart sensor technology for the maintenance of tomorrow and AI-supported low-cost robotics that are easy to operate. igus will also be presenting an AI-based app that shows design engineers the optimisation potential of their application with lubrication-free motion plastics in a matter of seconds.