Large space, small price: motion plastics make igus delta robots cost-effective and low-maintenance

Published on: October 9, 2019

Simple automation and low cost: the igus delta robot makes this possible by the use of lubrication-free components made of tribo-polymers. At the 2019 Motek show, the motion plastics specialist presented a new version with a 10 times larger work space volume compared with the proven model. This lightweight system for easy pick & place tasks, is delivered as a pre-assembled kit or ready to install product. This guarantees quick operation and saves costs immediately.

Read more...

Bigger, stronger, faster: new igus linear robots for cost-effective automation

Published on: October 9, 2019

Simple, precise, fast processes: these are the requirements of Cartesian robots. They are used for such things as pick-and-place applications, sorting systems and medical technology. igus has now developed a linear and room linear robot for large workspaces. The two new kinematics systems allow users to move up to five kilogrammes. Both linear robots are available directly from stock. They can also be customised to suit the customer application in question – no minimum order quantity.

Read more...

7th vector award: expert jury is looking for exciting energy chain applications

Published on: October 8, 2019

While many stars and starlets can hardly wait for the spotlight of an awards ceremony, designers do not often rush into the limelight. But the jury of experts at the vector award is certain that it is precisely they and their innovations that deserve attention – after all, they shape everyday life in the industry and far beyond. That’s why developers are called upon to compete for the 7th vector award with their bold and extraordinary energy chain applications.

Read more...

Rotary movements up to 7,000 degrees in extremely small spaces with twisterband HD

Published on: October 2, 2019

igus has developed the twisterband HD so that cables and hoses can be guided safely and reliably even during rotary movements. The lightweight energy chain is very stable, easy to fill and can even cope with rotating speeds of up to 180 degrees a second. It rotates around its own axis. Due to the long service life of the series, igus has now added two further sizes to the twisterband HD product range, these new sizes being intended for especially small installation spaces.

Read more...

Video: Revolutionary method of chain assembly

Published on: September 18, 2019

High unsupported lengths and long travels with large fill weights create extreme stress on energy chains. igus, the motion plastics specialist, has developed the E4Q energy chain series to tackle this. Based on the robust and proven E4.1 energy chain standard, the new range brings a long service life and a high degree of modularity.

Read more...