It undertakes work that is lethal for humans: the remote-controlled robot “Crawler” restores the inner walls of pipelines in power plants. An automation that needs to be regularly maintained in order to protect the power and data cables from the harsh environmental conditions. Here, the US manufacturer Remote Orbital Installations LLC relies on the collaboration with igus.
Classic clamps provide strain relief for pneumatic hoses in energy chains. But if they are over tightened, the hoses can be crushed. This can lead to a loss of performance. The answer from igus: a new CFX series clamp with high holding force, which at the same time makes over-tightening impossible.
In the industry, sparks due to a lack of electrostatic discharge can lead to expensive breakdowns of machines and systems and worst case explosions. In order to increase protection here, igus has expanded the range of lubrication and maintenance-free xiros guide rollers to include a dissipative variant made of stainless steel.
igus extends its range of iglidur tribological plain bearings for applications with special loads. The materials iglidur M210 and M260 are new to the range. They enable a quick changeover from thick-walled metal bearings to plastic bearings without any structural modifications. The advantage of a change is that the bearing points no longer require lubrication and are almost maintenance-free. They offer a significant time and cost advantage, especially in harsh environments in the daily operation of construction, agricultural and municipal machines.
Nature is often the best model: The shape of the new igubal pillow block is based on the design principles of a tree. Flattened radii ensure maximum resistance to mechanical stresses. This bionic shape makes the housings with their high-performance plastics that require no lubrication or maintenance a real alternative to classic cast iron housing bearings.