On the way to the championship: RoboCup Junior takes place at igus in Cologne

Published on: January 22, 2024

On Saturday, 27th January 2024, igus will open its doors in Cologne for the RoboCup Junior competition. Pupils from the Rhineland compete against each other with their self-built robots in various disciplines to prepare their qualification for the German Championships. Interested spectators and members of the press are very welcome.

Read more...

igus is once again looking for creative Low Cost Automation projects with the fastest return on investment

Published on: January 15, 2024

The German economy is weakening and will only recover slowly in 2024, according to the Institute for Macroeconomics and Business Cycle Research (IMK). The mechanical engineering industry is also feeling the effects. To strengthen competitiveness, organisations will have to focus on automation. Thanks to Low Cost Automation (LCA) and the RBTX robotics marketplace from igus, companies of all sizes can find a complete solution that suits their requirements and budget – from as little as €2,000. The plastics company is now honouring the projects with the fastest return on investment (ROI) with the ROIBOT Award for the third time. Users can now apply to win LCA products worth €5,000 in addition to international recognition.

Read more...

igus launches first UL-listed motor cable for cable tray and e-chain

Published on: January 10, 2024

With the new chainflex cable CF33.UL, igus has developed the world’s first motor cable for energy chains and cable trays with UL approval and a four-year functional guarantee in the energy chain. This allows the cable to be laid seamlessly from the energy chain to the cable tray without a plug connection in between. The CF33.UL also adds a shielded PVC motor cable to the chainflex range.

Read more...

igus fixed flange bearings become intelligent

Published on: January 8, 2024

Expensive machine and vehicle breakdowns due to undetected faults in heavy-duty fixed flange bearings: these will soon be a thing of the past thanks to a new generation of two- and four-hole fixed flange bearings. Their special feature is that the bearings, which are made of lubrication-free high-performance plastic, are equipped with miniature wireless sensors, enabling condition monitoring and predictive maintenance.

Read more...

Productivity up by 20%, cycle time down: igus sprue separator for injection-moulding machines

Published on: November 29, 2023

Increase efficiency while reducing costs: more and more companies are pursuing this goal in the course of Industry 4.0 so as to remain competitive. The automation of recurring production processes plays a central role in this process – also in injection-moulding production. Removing sprue often takes valuable time. The plastics specialist igus has therefore now developed a low-cost sprue separator for manufacturers of injection-moulding machines, such as Dr. Boy.

Read more...