Category:

Topteaser

3D printer builds houses from clay

Published on: February 20, 2026

Creating affordable living space in off-grid regions: this is possible thanks to a large-format 3D printer from the Italian company WASP, which uses clay to build house walls. To ensure that the printer can carry out this work reliably and without constant service and despite high dust and dirt loads, the engineers rely on lubrication-free liners made of high-performance plastic from igus in the machine’s mechanics.

Read more...

PFAS-tested: new dryspin® lead screw nut for quick replacement

Published on: February 8, 2026

Design engineers who want to replace the lead screw nuts of lead screw drives with PFAS-tested alternatives often face a dilemma: there are hardly any versions that are free of the controversial chemical, meaning that expensive adaptations would be necessary. igus is changing this with a new PTFE-free and PFAS-tested universal flange lead screw nut made of iglidur high-performance plastic. It allows a quick 1:1 conversion and promises an above-average service life thanks to a special thread geometry.

Read more...

3D-printed parts with injection-moulding quality: igus expands its portfolio of 3D printing filaments

Published on: February 4, 2026

If wear-resistant components made of high-performance plastics are required, igus offers the right choice from over 50 different materials for injection moulding. The 3D printing service comes into play for the cost-effective and fast production of components with special shapes, prototypes or small batches. igus has now added iglidur i190PF to its filament range so that customers can now also easily obtain extremely strong, wear-resistant and PTFE-free components from 3D printing.

Read more...

igus sets a new standard with the first online tool for the automatic design of Clean Cables

Published on: February 2, 2026

Cleanrooms for the production of microchips and semiconductors are characterised across the globe by the absence of particles and limited space. To safely guide cables under these conditions, igus has developed the e-skin flat. The new e-skin flat configurator now allows for the fast and automated design of flat cable guide systems in cleanrooms. This reduces the previously manual effort to just a few minutes. Users can configure a complete system, have it filled automatically and then immediately download a technical drawing and parts list. With the e-skin flat, which is suitable for dry cleanrooms, igus has now also received the “Best of Industry Award 2025” in the category battery development and production.

Read more...

Space-saving, abrasion-resistant and dissipative: compact e-skin soft ESD for cleanrooms

Published on: January 18, 2026

The demand for electric cars and the use of AI are growing, so that more and more lithium-ion batteries and microchips are required. As these technologies have to deliver performance that continues to increase, they are also becoming more sensitive and place high demands on production environments. With the e-skin soft ESD, igus is now launching a new energy chain for cleanrooms that is both abrasion-resistant and dissipative. It is a game changer for design engineers as it allows for significantly more flexibility and saves space in energy supply systems.

Read more...

Maximum performance in the smallest of spaces thanks to new miniature linear module with lead screw drive

Published on: January 14, 2026

Design engineers in medical technology and laboratory automation often face a problem: linear modules for positioning tasks with stroke lengths of over 200mm quickly become bulky, run unevenly due to the small lead screw diameters and do not fulfil the strict hygiene guidelines because of the lubricating grease. igus has therefore launched drylin SLW-0620-Ds08. The compact linear module with lead screw drive allows for smooth stroke lengths of up to 300mm, operates completely without lubrication and is PTFE-free and tested for PFAS.

Read more...

Reliable linear technology for Christmas magic without downtime

Published on: December 19, 2025

The facade of the French luxury fashion house DIOR enchants hundreds of thousands of people every year. What they don’t see: for the winter magic, design engineers have to overcome a number of challenges, such as finding electrical adjustment systems for the moving figures that also work in freezing temperatures. Weather-resistant and lubrication-free linear modules from igus ensure trouble-free Christmas magic.

Read more...

238 chainflex cables receive certificate for use in dry cleanrooms

Published on: December 17, 2025

Around the world, the number of dry cleanrooms is increasing. The main focus is on automating the systems to ensure fast and cost-effective production. In addition to its certified energy chains suitable for dry cleanrooms, igus has now also had its halogen-free chainflex TPE cables successfully certified by the Fraunhofer Institute for Manufacturing Engineering and Automation (IPA) in accordance with dry cleanroom Classes 4 and 5. This provides customers in highly automated battery production with energy management solutions with a reliable guaranteed service life of up to four years.

Read more...

New control unit from igus accelerates prototype development

Published on: December 11, 2025

Testing linear systems with stepper motors in just a few minutes before installation: the new drylin control unit from igus makes this possible. The compact drylin DLE-CU-9 eliminates the need for tedious cabling with separate control and IT systems, speeding up the commissioning of series machines and the development of prototypes. It is also a fully-fledged solution for simple automation tasks.

Read more...

When the robot monitors itself

Published on: November 27, 2025

Unplanned downtimes in automation not only cost time, but also money – especially in the automotive industry. With the new TR.P sensor, igus is launching a smart solution for industrial robots that actively monitors triflex energy chain systems and reacts immediately to critical tensile forces. The system recognises potential damage at an early stage, increases operational safety and provides support during commissioning through condition monitoring. igus will present the new solution at the SPS in Nuremberg (Hall 4, Stand 310).

Read more...