Low-Cost-Automation
igus has added a new AI chatbot to the online platform RBTX.com. The interactive consultant is designed to enable companies with little previous experience and technological expertise to quickly and reliably put together Low Cost Automation (LCA) solutions to become more competitive. First users are enthusiastic about the intuitive AI solution.
Whether you’re visiting the Christmas market with friends or enjoying Christmas dinner with family, a good mulled or special wine is a must. To offer people this supposed matter of course even in times of labour shortages, winemakers must increasingly rely on automation during the grape harvest. However, slopes with a gradient of 75% and narrow rows of vines were previously considered impossible to automate. The German company CH engineering GmbH has developed a particularly compact harvesting vehicle for precisely this area of application. It uses a robust energy chain made of high-performance plastic from igus to work reliably even under difficult conditions, minimising maintenance work for winemakers.
With the new ReBeL Move, which the Cologne-based motion plastics specialist is presenting at Motek 2024, igus proves that the automation of material-handling processes doesn’t have to be expensive or complicated. The mobile robot moves autonomously through factory halls, transporting products from one place to another. It can also be combined with the ReBeL Cobot made of high-performance plastic. It only takes users with even the most basic IT skills an hour to commission and is available – including the ReBeL Cobot – for €34,808 (prices may differ in your country).
A hackathon took place at the igus headquarters in Cologne in mid-September. In line with the motto “Artificial intelligence meets robotics”, 17 participants worked in three interdisciplinary teams to develop advanced automation solutions for logistics. The aim of the hackathon was to create an automated method for packing up pizzas using a large language model (LLM for short) based on AI. The event was organised in cooperation with the Fraunhofer Institute for Intelligent Analysis and Information Systems IAIS, the University of Bonn, the Lamarr Institute and the Fraunhofer Institute for Material Flow and Logistics IML.
After a long day at the beach, enjoy your hotel room with a drink from the good old minibar. This is very different in some hotels. To the surprise of the guests, JEEVES shows up – a robot from the Munich-based company Robotise Technologies GmbH. The waitressing service robot replaces up to 300 minibars and relieves hotels in times of a shortage of skilled labour. The engineers rely on space-saving and fail-safe energy chains from igus to guide the sensitive energy and data cables so that they can do their job without disruption.
Bikes instead of cars: for the mobility transition to work, cities need more parking facilities without encroaching too much impact on the cityscape. For this purpose, the Japanese manufacturer Giken has built a garage called Eco Cycle, which parks bicycles completely automatically underground. To ensure the reliability of the robot garage, the engineers used robust and maintenance-free energy chains from igus for the lift’s cable guidance system.
With the growing demand for electric cars, the need for high-quality lithium-ion batteries is also increasing. For this reason, they should ideally be manufactured in dry cleanrooms with minimal humidity and as little particulate matter as possible. At the same time, this environment must be automated because people are not allowed to spend long periods of time in dry cleanrooms. To ensure safe and reliable energy supply to robots, motion plastics specialist igus has developed the triflex R TRC: the first robot energy supply system with a certification for dry cleanrooms from Fraunhofer IPA for ISO Class 4-5.
Robots have become an integral part of industry and are increasingly finding their way into small and medium-sized companies in the form of cobots, such as the ReBeL. They sort, pick and move with the help of cameras, suction devices and gripper systems. igus has now developed a finger gripper for the ReBeL cobot so that it can also perform humanoid tasks. It is made entirely of lubrication-free plastics, and is therefore very cost-effective and easy to integrate.
It is affordable, compact, lightweight and ready to install with a mouse click: igus has added a minimalist low-cost variant to the portfolio of its iglidur PRT series of slewing ring bearings. The PRT-05-15-PC not only reduces costs, but also protects the environment. The new slewing ring bearing consists of 97% regranulated high-performance plastics.
Accountants, journalists and even computer scientists are all amazed at how rapidly automation is developing, including with artificial intelligence. Industry representatives are, too. They are drawing new ideas for smart factories. Many traditional SMEs, however, are in danger of falling behind. Low Cost Automation can provide immediate assistance and help them avoid missing the boat.