New igus adapter reduces assembly time of energy chains by 80%

Published on: October 29, 2020

Connecting cables individually not only takes time, but is also prone to errors. This is why igus has developed the Module Connect interface concept, with which energy chains can be easily plugged together. To connect the connector to the energy chain, the user can now use an individual adapter. The energy chain thus becomes an interface that saves 80 per cent of the installation time. The design and functionality of the adapter also convinced the jury of the German Design Award 2021.

Read more...

Switch-off protection on long travels: new EC.PR system monitors energy chains

Published on: October 29, 2020

A forgotten screwdriver in an energy chain, a bent trough as well as ice, snow and bulk material can quickly lead to a total failure of cranes with high costs. This prompted igus to develop a new push/pull force monitoring system. The EC.PR precisely records the force values of the floating moving end and adjusts the force limits. This prevents high repair costs and damage to the system.

Read more...

Unique plastic plain bearing applications wanted!

Published on: October 22, 2020

An offshore inspection device, a floating catamaran and a driver assistance system for people with reduced mobility. What they have in common is the extraordinary use of high-performance plastics in bearing technology with which they won the 2019 manus award. A joint initiative, which the plastics specialist igus announces every two years, is now looking for unique applications with plastic plain bearings. The winner will receive prize money of up to 5,000 euros. To mark the tenth anniversary of the manus award, the jury is offering a sustainability prize.

Read more...

Simply off the roll: new chainflex cable box saves 84 per cent shipping costs

Published on: October 9, 2020

igus has developed a new logistics solution for its special energy chain cables. With the chainflex CASE, the user directly saves several times over, because instead of delivery by a courier, the cable now comes by parcel service in a secure stackable box. This significantly reduces both shipping and storage costs. The cable can be unreeled straight from the box and cut to the desired length. A QR code on the chainflex CASE ensures that the cable can be re-ordered quickly.

Read more...

Harnessing the secrets of nature: the E4Q energy chain from igus wins the German Design Award

Published on: October 9, 2020

The E4Q energy chain series was developed by igus to achieve the best possible solution for unsupported and long travels. In the process, shapes inspired by nature ensure very low weight, while a unique tool-free opening concept reduces installation time by 40 per cent. The E4Q has now received the renowned German Design Award for this pioneering design.

Read more...