igus is expanding its range of harnessed readycable for moving industrial applications. New additions to the portfolio are cables with plug connections for systems from Keyence, one of the world’s leading manufacturers of automation and quality assurance solutions. Designers can immediately connect the ready-to-connect cables to moving high-speed cameras using the plug-and-play principle, for example, and thus make them even more fail-safe – without time-consuming and error-prone in-house designs.
The AX-1 robot from Norwegian start-up Kilter applies herbicides to weeds with such precision that the use of chemicals is reduced by up to 95% – thanks to AI and sensor technology. To ensure that the autonomous helper is also gentle on the soil, the developers rely on lightweight and lubrication-free linear technology from the igus drylin series.
Customised automation doesn’t have to be expensive. Metaprint AS from Estonia, one of the largest manufacturers of aerosol packaging in Europe, demonstrates this. The company now uses an XXL linear robot from igus to load a printing machine. Compared to conventional systems, this Low Cost Automation solution reduces investment costs and is also easy to put into operation thanks to the plug & program function.
The efficient use of loading space is becoming increasingly important in view of the growing volume of lorry traffic on German roads. igus has therefore developed the new readychain eco-rack. The transport and assembly rack for pre-fitted energy chains consists of strong multiplex panels made of birch wood. In contrast to classic metal racks, it can be dismantled without tools. During return transport, it saves up to 88% of the original transport volume, reducing CO₂ consumption and transport costs. The eco-rack is now available for customers of the readychain service.
3D printing, CNC production or injection moulding? When design engineers are looking for the most suitable manufacturing process for a customised component, they often lose track of things, which costs valuable time. The igus tribo-parts service changes this: a free online tool that enables design engineers to find the most efficient manufacturing process in terms of cost, delivery time and service life for the required component – with just a few clicks and on one page.