In the area of machine tools, many users around the world rely on Fanuc motors and control systems. In order to reliably supply the drives with energy while they are in motion, igus has now developed a highly flexible servo cable. It is designed specifically for use in dynamic applications. The cable has an oil-resistant PUR jacket, UL certification, and a UL-verified, certified guarantee promise for up to 36 months.
The new generations of cranes demand increasingly more from energy supply systems. Now an energy chain meets precisely these requirements for longer travels, higher accelerations and speeds as well as reliability. The new heavy-duty P4HD rol e-chain is made of highly abrasion-resistant materials. Special side parts, newly designed joining links, roller links as well as a triple stop-dog system minimise wear and reduce the drive energy even further. All parts can be replaced in case of maintenance. To monitor the service life, smart plastics sensors can be integrated into the pin/bore connection.
In 1964, they founded igus in their back yard garage in Cologne-Mülheim. In 2021, the internationally active company supplies customers all over the world with its lubrication-free and maintenance-free motion plastics. On the occasion of the founders’ 90th birthday, igus is bringing that garage back to life.
igus, a motion plastics specialist, showcases what plastics can do with its first drylin W linear bearing made entirely of tribo-polymers. The linear bearing has been developed specifically for linear movements. At just ten grammes, it is quick to install, vibration-dampening, lubrication-free and ideal for transportable applications. The fact that it is injection moulded makes it very cost-effective. The injection moulding-optimised design also reduces its weight, lowering the necessary linear system drive energy.
Solarmid and iglidur P UV are the names of the two new materials that igus has now developed specifically for pillow blocks in single-axis solar trackers. The new polymer’s durability is showcased particularly well in 2P (two-in-portrait) tracker applications, which subject bearings to direct sunlight for hours at a time. The materials were convincing in real-life testing, exhibiting up to three times the UV-resistance.