Hygienically designed slewing ring bearings have been scarce on the market. Manufacturers of special machines for hygiene-sensitive areas therefore often have to design additional covers. However, igus is now changing all that – with a hygienically designed iglidur PRT slewing ring bearing that enables quick, residue-free cleaning during use. This slewing ring bearing can remain permanently installed in an application with food contact, saving the user the effort of developing a suitable cover.
A wide, angular frame made of plastic, black wheels with Y-spokes: The futuristic look of the bike designed by mtrl, a Dutch bicycle developer, with motion plastics from igus has won the prestigious German Design Award 2023. The award brings an important step in realising the sustainability vision of a bicycle production with post-consumer-waste recycled plastic for urban mobility.
igus is launching the drylin Endless Gear linear module (EGW), a modular, lubrication-free linear guide with rack and pinion drive. The modular system can be extended to any travel length, costs little and is almost as light as the guide for a toy train. Several carriages can travel on it in different directions and at different speeds. Users can also extend the linear guide after installation and add more carriages.
Cleanroom-compatible energy chains from the e-skin flat series still qualify for the highest cleanroom class even after 1.5 years of continuous use and 60 million double strokes. A test, unprecedented in the industry, led to this result. It was carried out in a cleanroom laboratory set up by motion plastics specialist igus in cooperation with the Fraunhofer Institute for Manufacturing Engineering and Automation (IPA).
Maintaining heavily used and hard-to-reach bus cables faster than ever is what i.Sense CF.D, the igus monitoring module, can do – and nothing else in the world can. The module automatically recognises the positions of stressed areas in a cable and shows them very precisely in metres. The new optical status display now enables users to intervene quickly in a targeted manner, avoiding time-consuming and costly troubleshooting.