Reduce costs for indoor cranes by up to 40% with new igus glide-chain

Published on: March 27, 2025

The energy chain specialist igus is presenting its new energy chain called “glide-chain” at the Hannover Messe. It has been developed specifically for gliding applications and is ideal for travels of up to 30m, as is the case with indoor cranes, for example. Its slim design ensures cost savings of 30 to 40%.

Read more...

Surgical microscope for structurally weak countries wins manus plastic bearing competition 2025

Published on: March 27, 2025

A mobile surgical microscope from Prechtl Tech Solutions for structurally weak countries has won the manus plastic bearing competition 2025. A jury of experts recognised the engineers who used lubrication-free polymer bearings and were thus able to increase the reliability of the microscope. Other winners of the competition include a bicycle trailer for parcel delivery, an AI hoe for agriculture and an agrivoltaics system with irrigation and cultivation system. They have all created ecological, economic and social benefits by switching to lubrication-free plain bearings made from high-performance plastics.

Read more...

igus reaches one-billion mark in sales and increases the number of active customers by 5%

Published on: March 25, 2025

With 277 motion plastics innovations in 2025, igus is presenting a record number of new lubrication-free plastic products in line with the motto “GO ZERO Lubrication”: from PTFE-free materials and a complete energy chain series made of recycled materials to a new type of dry cleanroom certificate and a humanoid robot. This is the result of continuous investment in research and development to offer customers state-of-the-art solutions. Despite the challenging geopolitical and economic situation in 2024, the motion plastics specialist was able to increase the number of active customers by 5% and maintain its billion-euro turnover. With sales of €1.105 billion, the company recorded a comparatively moderate decline in turnover of 2.5%.

Read more...

Now it’s clicked: PTFE-free positional system from igus for precise adjustment

Published on: March 20, 2025

Whether moving to specified spots with a sensor, adjusting a headrest to the desired height or getting a screen into an ergonomic position until it clicks: igus has launched the new linear guide with PTFE-free drylin WWP locking carriages for simple positioning tasks, e.g. in the interior. The solution is intuitive, compact, durable and, thanks to the material combination of lubrication-free high-performance plastics and aluminium, particularly light, hygienic and low-maintenance.

Read more...

This robot piggybacks 600kg shelves

Published on: March 11, 2025

The French company SCALLOG has developed an autonomous robot called “Boby” that can transport shelves weighing up to 600kg in logistics warehouses. To maximise the robot’s range and minimise maintenance, the engineers rely on lubrication-free iglidur plain bearings from plastics specialist igus, which are wear-resistant and significantly lighter than comparable metal solutions.

Read more...