igus expands D1 motor control with certified PROFINET

Published on: May 22, 2025

igus increases the flexibility of its D1 motor control, which designers use for electric linear drives, handling systems and robot axes. It is now possible to integrate the D1 seamlessly and quickly into higher-level control systems from Siemens, Beckhoff, Wago and other manufacturers using Siemens-certified PROFINET – without time-consuming and complicated adaptations. This extended connectivity should significantly increase the performance and efficiency of automation processes.

Read more...

For less than €50,000*: igus presents humanoid robot Iggy Rob

Published on: May 7, 2025

Humanoid robots are on the verge of revolutionising the industry. While previous systems are very expensive, motion plastics specialist igus is now offering its first humanoid robot, Iggy Rob, as a low-cost solution. For €47,999, it supports companies in industrial production, service or with transport tasks. To gain experience with the new helper, igus is calling on companies to “test before they invest”.

Read more...

igus launches wear-resistant plain bearing range without PTFE

Published on: April 30, 2025

Just in time for Hannover Messe, igus is announcing a breakthrough: the material developers in Cologne have succeeded in producing the established polymer plain bearings from the iglidur G, iglidur X and iglidur H series, which are used in machines, systems and vehicles worldwide, without PTFE. This is good news for a lot of companies that are already looking for future-proof alternatives due to the prospect of stricter PFAS regulations or even a ban.

Read more...

Safety in battery production due to long-term tests: new dry-cleanroom certificates for igus e-chains

Published on: April 23, 2025

Two years ago, igus presented the E6.29, the first certified energy chain for dry cleanrooms. In order to offer customers long-term security, the motion plastics specialist commissioned the Fraunhofer IPA to carry out a test to investigate the ageing behaviour of its e-chains in the dry cleanroom – with positive results. Together with the IPA, the company has now developed new certificates that confirm the suitability of the energy chains E6, e-skin flat, e-skin soft and easy chain E14 for dry cleanrooms in long-term tests.

Read more...

80% lower CO2 footprint: igus switches to recycled material for energy chain series E2.1

Published on: April 16, 2025

Following the successful development of the world’s first energy chain made from recycled plastic, motion plastics specialist igus is taking the next step: the company is converting the entire catalogue range of its standard energy chain series E2.1 to the new recycled material igumid CG LW.

Read more...