Surfing on land: motion plastics keep people and machines fit

Published on: October 26, 2019

For the designers of Surf Evolution, the metallic bearings proved to be too maintenance-intensive and too expensive in their novel surf machines. Looking for an alternative, they quickly came across the motion plastics from igus. And the design engineers were thrilled, because the retrofitting significantly reduced the maintenance and saved 70 per cent in costs.

Read more...

3,022km through the desert! With solar power and lightweight igus plain bearings in solar racing cars

Published on: October 23, 2019

The goal of the World Solar Challenge was to cover 3,022 kilometres of the Australian desert powered only by the sun. One of the participants was Team Sonnenwagen from Aachen. To develop their solar-powered car, the students relied on the lightweight, wear-resistant and lubrication-free iglidur plain bearing technology made of durable tribo-polymers from igus. This enabled the team to comfortably finish sixth in the race.

Read more...

Vertical instead of horizontal: how motion plastics make agriculture sustainable

Published on: October 17, 2019

According to the United Nations, world population will grow to 9.7 billion by 2050. In particular, the population of the cities will increase significantly. Vertical farming is considered a promising alternative to conventional methods to produce food for the growing number of urban dwellers, reliably and cost-effectively. In these vertical farms, motion plastics from igus already play a major role in their cost-efficient and reliable operation.

Read more...

Electrostatically dissipative: igus polymer ball transfer units ensure safe conveyance of products

Published on: October 15, 2019

Users rely on ball tables for transducers in roller conveyors and for the transport of sensitive goods. Here igus polymer ball transfer units are used, because they can even move loads up to 500N smoothly and in all directions without any lubricant. To protect both conveyed goods and people from uncontrolled static electricity discharge, igus has now developed the tribo-polymer xirodur F182 for its ball transfer units. The new material is extremely durable and has proved its electrostatic conductivity in tests.

Read more...

Large space, small price: motion plastics make igus delta robots cost-effective and low-maintenance

Published on: October 9, 2019

Simple automation and low cost: the igus delta robot makes this possible by the use of lubrication-free components made of tribo-polymers. At the 2019 Motek show, the motion plastics specialist presented a new version with a 10 times larger work space volume compared with the proven model. This lightweight system for easy pick & place tasks, is delivered as a pre-assembled kit or ready to install product. This guarantees quick operation and saves costs immediately.

Read more...

Bigger, stronger, faster: new igus linear robots for cost-effective automation

Published on: October 9, 2019

Simple, precise, fast processes: these are the requirements of Cartesian robots. They are used for such things as pick-and-place applications, sorting systems and medical technology. igus has now developed a linear and room linear robot for large workspaces. The two new kinematics systems allow users to move up to five kilogrammes. Both linear robots are available directly from stock. They can also be customised to suit the customer application in question – no minimum order quantity.

Read more...

7th vector award: expert jury is looking for exciting energy chain applications

Published on: October 8, 2019

While many stars and starlets can hardly wait for the spotlight of an awards ceremony, designers do not often rush into the limelight. But the jury of experts at the vector award is certain that it is precisely they and their innovations that deserve attention – after all, they shape everyday life in the industry and far beyond. That’s why developers are called upon to compete for the 7th vector award with their bold and extraordinary energy chain applications.

Read more...

Rotary movements up to 7,000 degrees in extremely small spaces with twisterband HD

Published on: October 2, 2019

igus has developed the twisterband HD so that cables and hoses can be guided safely and reliably even during rotary movements. The lightweight energy chain is very stable, easy to fill and can even cope with rotating speeds of up to 180 degrees a second. It rotates around its own axis. Due to the long service life of the series, igus has now added two further sizes to the twisterband HD product range, these new sizes being intended for especially small installation spaces.

Read more...