Keyword:

Motek

7th vector award: expert jury is looking for exciting energy chain applications

Published on: October 8, 2019

While many stars and starlets can hardly wait for the spotlight of an awards ceremony, designers do not often rush into the limelight. But the jury of experts at the vector award is certain that it is precisely they and their innovations that deserve attention – after all, they shape everyday life in the industry and far beyond. That’s why developers are called upon to compete for the 7th vector award with their bold and extraordinary energy chain applications.

Read more...

Rotary movements up to 7,000 degrees in extremely small spaces with twisterband HD

Published on: October 2, 2019

igus has developed the twisterband HD so that cables and hoses can be guided safely and reliably even during rotary movements. The lightweight energy chain is very stable, easy to fill and can even cope with rotating speeds of up to 180 degrees a second. It rotates around its own axis. Due to the long service life of the series, igus has now added two further sizes to the twisterband HD product range, these new sizes being intended for especially small installation spaces.

Read more...