e-chains
Whenever the highest hygiene standards are required, igus scores high with lubrication-free and abrasion-resistant plastic components for movement. In particular, battery production for tomorrow’s mobility requires special environmental conditions, which are achieved through the combination of dry rooms and cleanrooms. The Fraunhofer IPA has developed a new type of certificate for precisely these requirements. The E6.29 energy chain from igus is the very first cable guide system that has been tested under dry cleanroom conditions and has now been certified with ISO Class 4.
Cleanroom-compatible energy chains from the e-skin flat series still qualify for the highest cleanroom class even after 1.5 years of continuous use and 60 million double strokes. A test, unprecedented in the industry, led to this result. It was carried out in a cleanroom laboratory set up by motion plastics specialist igus in cooperation with the Fraunhofer Institute for Manufacturing Engineering and Automation (IPA).
Save installation space and weight with just one cable for power and data: it’s easy with harnessed igus readycable hybrid cables. New to the range are ready-to-connect cables suitable for SEW-EURODRIVE with MOVILINK DDI and Siemens SINAMICS S210 with OCC. In addition to PUR, the latter is also available with an outer jacket made of cost-effective PVC. Macros for the EPLAN Electric P8 software speed up cable planning by around 50%.