Linear technology
In order to move doors, monitors or even panels, users rely on lateral installation of the linear systems. To enable the linear guides to absorb these lateral forces better, igus has now developed a new hybrid linear system. Two hybrid bearings provide low-friction adjustment with polymer rollers and tribo-polymer slide elements. Combined with an easily fit rail adapted to the new roller bearings, igus offers a cost-effective and visually appealing complete solution.
igus has developed a new self-lubricating, two-component bearing, iglide Q2E, that can withstand the extreme conditions frequently found in agricultural machines, utility vehicles, offshore installations and other demanding environments.
Designing the right shaft for an application is not easy without CAD software and in-depth technical knowledge. igus has now developed a new, free-of-charge and freely accessible online tool with the drylin shaft configurator. In just three steps, the user is given the opportunity to select the right shaft in the required length from seven materials, machine the main body and the machined ends with standard elements such as chamfers and grooves and order the configuration. In addition, the user receives the STEP files of their configuration as well as a dimension drawing for download, free of charge.
High speeds and high waves not only make for a lot of fun on board high-speed boats, they can also be dangerous as passengers experience a physical shock every time the boat’s hull strikes the water. Vibration-dampening seats with bearings that absorb these shocks are therefore called for. Designers are able to rely on wear-resistant igus linear bearing technology, thanks to the use of tribo-polymers that are lubrication-free, maintenance-free and corrosion-free.
Fast automation in confined installation spaces: igus has now developed an extra-compact toothed belt axis based on its flat drylin N linear system. The new axis consists of a completely standard fitment of components and is thus easily assembled within a few minutes and cost-effective. Equipped with motor and control, the new system can carry loads of up to 20 Newton and a translation of 60 millimetres per revolution.