Energy chains
Smart monitoring of igus bus and data cables goes into the next round: the latest generation of i.Sense CF.D monitoring sensors checks the electrical condition of chainflex cables in e-chain systems – without contact and without intervention in the existing harnessing. This allows real-time monitoring without any extra cores and, in combination with the new i.Cee: plus II evaluation module, allows even more efficient predictive maintenance for protection against expensive system failures.
It is light, compact, and made entirely of plastic: the new PRM (Polymer Rotation Module) rotary energy supply system from igus. Specifically for tight rotational movements in cables and hoses, igus has now developed a system consisting of a polymer energy chain and a low-friction plastic guide trough. Users can increase the service life of their machines and systems with buying costs up to 73% less than those of a comparable steel guide trough. The new e-chain system expands the igus range of complete sets that can be ordered directly online.
Particle-free energy chains are required to guide cables and hoses safely in cleanrooms. igus developed the e-skin flat, a modular design, a cost-effective alternative to ribbon cables. In the Fraunhofer cleanroom test, the energy supply system has proved its freedom from particles in accordance with ISO Class 1 not only as a single-layer, but also as a three-layered ready-to-connect energy chain system.
The Drop Station is a new sustainable beverage vending machine that fills compostable containers with customised beverages at the touch of a button. The water for the vending machine does not need to be transported, since the kiosk can be connected to a water source on site. A linear robot with drylin linear guides mixes the beverages and dispenses them. Harnessed e-chains ensure protection for the chainflex energy and data cables.
The new generations of cranes demand increasingly more from energy supply systems. Now an energy chain meets precisely these requirements for longer travels, higher accelerations and speeds as well as reliability. The new heavy-duty P4HD rol e-chain is made of highly abrasion-resistant materials. Special side parts, newly designed joining links, roller links as well as a triple stop-dog system minimise wear and reduce the drive energy even further. All parts can be replaced in case of maintenance. To monitor the service life, smart plastics sensors can be integrated into the pin/bore connection.
On long travels, the energy supply systems from igus are favourites for safely guiding cables and hoses. In most applications, customers rely on the strong E4.1 universal energy chain modular system. igus has now expanded the successful system with glide pads and roller chain links for quick retrofitting. This allows users in abrasive environments as well as in applications with very high speeds or extreme travel lengths to increase the service life of their systems quickly and cost-effectively.
To ensure that cables on industrial robots can be guided in motion safely, easily and compactly, igus has now developed the four-dimensional triflex TRX energy chain. The new design study replaces classic robot hose packages and retraction systems. Special feature: 40 per cent retraction length ensured by a unique telescopic mechanism inside the chain. This allows users to save space on the third axis of their robot, up to 83 per cent weight and high costs for retraction systems.
High abrasion resistance is crucial for machine elements in cleanrooms. igus has therefore now developed the C6, an energy chain designed to meet the highest cleanroom class. The new chain is specially designed for longer unsupported applications on machines and systems, and is based on the successful E6 and E6.1 cleanroom series from igus. A new connector system and a specially tribologically optimised high-performance polymer make the design study from igus even smoother, easier to assemble and virtually free of any particles in motion.
If a component is to have several properties, it usually has to be manufactured in several steps. But such production can quickly become cost-intensive for small quantities. It is precisely for this reason that igus now offers multi-material printing with up to four materials. This allows multifunctional and wear-resistant special parts to be manufactured quickly and cost-effectively in just one step. To this end, igus has further expanded its 3D printing capacities and its range of materials for the FDM process.
High-purity manufacturing environments ensure that electronics also function safely in everyday life. In order for manufacturers to produce in cleanrooms, particle-free machine elements are required. Every year, the Fraunhofer Institute honours the most innovative developments with the REINER! Award. The motion plastics specialist igus is very pleased with the 2nd place award for its e-skin flat energy supply chain. The alternative to the flat belt guide is compact, modular and has cleanroom class 1. The cables can be easily inserted into the chain using the zipper principle and can be quickly replaced in the event of maintenance.