Energy chains
igus has added an ESD variant specifically for highly sensitive cleanrooms to its e-skin flat series. The modular ribbon cable’s new material prevents the chain from becoming electrostatically charged while ensuring that it generates no particles, even during very fast movements. The modular design with individual pods also allows quick energy supply system filling.
New addition to the igus energy chain portfolio: the E4Q, a globally proven e-chain for applications with large unsupported lengths and high fill weight, now has a new variant: the “L”. Users for whom the E4Q is too large can now save costs of up to 20% with the E4Q.64L. They will still benefit from the advantages of its big brother, such as quick, tool-free opening.
In production, downtimes are expensive. For manufacturers of such items as machine tools, it is therefore very important for system assembly work to be as quick and efficient as possible. The readychain rack is a modular assembly and transport rack for harnessed energy supply systems, one that igus has been offering for ten years. Now, igus has developed a solution that is even simpler and faster, with practically unlimited customisation potential: the first 3D-printed readychain p-rack (printed rack). It can be adapted to customer requirements with millimetre precision.
Things don’t have to be expensive. This is true not only of groceries, but also of energy chains. The simplest products often not only cost the least, but also represent the best technology. igus has now developed the snapchain 2.0 especially for low-stress and flat cable packages. The energy supply system consists of just one side link, to which cables can be fixed with cable tiewraps. It is made entirely of recyclate, so it is a sustainable solution.
Whenever the highest hygiene standards are required, igus scores high with lubrication-free and abrasion-resistant plastic components for movement. In particular, battery production for tomorrow’s mobility requires special environmental conditions, which are achieved through the combination of dry rooms and cleanrooms. The Fraunhofer IPA has developed a new type of certificate for precisely these requirements. The E6.29 energy chain from igus is the very first cable guide system that has been tested under dry cleanroom conditions and has now been certified with ISO Class 4.
In applications with loads of more than 80Mpa, plain bearings made of thermoplastic materials can be pushing their limits. igus has expanded the existing range of standard plain bearings with the new igutex fibre wound plain bearing series. The series displays its strength in heavy-duty areas such as construction machinery or hoists. The latest development in the product family is the material igutex TX3. It offers an even higher running performance with high dynamic forces than previous igutex bearings.
Energy and data cables hanging from jib cranes often pose a great risk. Careless movement of loads, forklifts or other slewing crane systems in the immediate vicinity can cause them to become entangled and torn off. igus has therefore developed the guidelok swing, the only energy supply system of its kind in the world. It can be installed directly in the T-beam contour, and a special rocker system allows it to be used for long beam lengths cost-effectively with little wear. This significantly increases operational safety.
To be able to safely guide large hoses, igus has now developed a new extender crossbar design for its E4Q modular energy chain series. With the help of an adapter system, the chain can be individually adapted to the hose diameter. The tool-free E4Q opening mechanism ensures easy installation and filling of the energy supply.
A quick and easy individual solution: igus, the motion plastics specialist, offers a wide range of online tools (among other things) to streamline the process. They include the “e-chain expert”, which enables interested parties to assemble an individual energy chain system in just three steps. Price, service life and delivery time are displayed. For the first time, users now have the option of configuring their e-chain with the intelligent i.Sense EC.W wear sensor directly. This gives customers a complex, ready-to-connect e-chain system that includes real-time condition monitoring – in just a few clicks.
Cleanroom-compatible energy chains from the e-skin flat series still qualify for the highest cleanroom class even after 1.5 years of continuous use and 60 million double strokes. A test, unprecedented in the industry, led to this result. It was carried out in a cleanroom laboratory set up by motion plastics specialist igus in cooperation with the Fraunhofer Institute for Manufacturing Engineering and Automation (IPA).