Print strong, abrasion-resistant parts easily yourself with the new igus tribo-filament

Published on: March 4, 2021

To manufacture wear-resistant parts in special dimensions quickly and cost-effectively, igus has now developed a new, easy-to-machine all-rounder filament: iglidur I190. It is remarkable for its great mechanical flexural strength (80 MPa). The tribologically optimised material requires no lubrication or maintenance and can be used with all commercially available 3D printers with heated printing plates.

Read more...

3D printing in outer space: igus linear axes produce spare parts in zero gravity

Published on: February 25, 2021

When booms for solar panels or satellite antennas are transported into space in a launch vehicle, they are exposed to high loads. To simplify the complex transport and speed up the production of the elements, the AIMIS-FYT student team is working on a 3D printing process. In the future, it should be possible to produce structural parts in outer space. To conduct experimental tests in zero gravity, the students built a 3D printer. For the drive technology supported by igus, they relied on the maintenance-free and lightweight drylin SAW linear axes.

Read more...

When speed is a must: igus FastLine delivers injection-moulded special plain bearings in 7 days

Published on: February 18, 2021

When the market demand for a product is high, then the manufacturers and their suppliers are needed. Customised parts, such as plain bearings in special shapes, have to be delivered quickly and without complications. But it is not unusual for the production of special parts by injection moulding to take several weeks. The plastics specialist igus therefore now offers its customers the FastLine Service thanks to its expanded in-house toolmaking department. Lubrication-free, polymer plain bearings in special dimensions can be delivered within a few days at cost-effective unit prices.

Read more...

Hannover Trade Show 2021: New modular gearbox kit from igus for innovative cobot ideas

Published on: February 11, 2021

The potential for service robotics is enormous: in kitchens and bars, in the area of nursing, or in agriculture and logistics, lightweight robots facilitate the automation of monotonous or non-ergonomic tasks. To make the implementation of such new concepts easy and, above all, cost-effective, igus is presenting a new modular gearbox kit for cobots at the Hannover Trade Show. The fully integrated tribo strain wave gear with motor, absolute-value encoder, force control system and controller is the main component of this kit.

Read more...

Securely sealed off! New interior separation for E4Q energy chain reduces assembly time

Published on: February 4, 2021

For safe cable guidance in unsupported and long travels, igus has developed the E4Q energy chain. The bionically inspired design of the series saves weight, while a crossbar with locking tabs reduces the assembly time of the energy supply system by 40 per cent. To further facilitate cable filling, igus is now launching a new interior separation for the E4Q. Universal separators can simply be placed on the crossbars, shelves can be inserted from the left or right, either along the inner or outer radius. A mechanism in the separators automatically locks the chain when closing.

Read more...