4K for 3D: igus offers multi-material printing for multifunctional components

Published on: May 6, 2021

If a component is to have several properties, it usually has to be manufactured in several steps. But such production can quickly become cost-intensive for small quantities. It is precisely for this reason that igus now offers multi-material printing with up to four materials. This allows multifunctional and wear-resistant special parts to be manufactured quickly and cost-effectively in just one step. To this end, igus has further expanded its 3D printing capacities and its range of materials for the FDM process.

Read more...

C6 e-chain: new design and abrasion-optimised materials for cleanrooms of the highest class

Published on: May 6, 2021

High abrasion resistance is crucial for machine elements in cleanrooms. igus has therefore now developed the C6, an energy chain designed to meet the highest cleanroom class. The new chain is specially designed for longer unsupported applications on machines and systems, and is based on the successful E6 and E6.1 cleanroom series from igus. A new connector system and a specially tribologically optimised high-performance polymer make the design study from igus even smoother, easier to assemble and virtually free of any particles in motion.

Read more...

iglidur I151 for FDA-compliant, detectable, wear-resistant parts in food technology

Published on: April 29, 2021

iglidur I151 is blue, prints easily, and has an optimal coefficient of friction and wear. The new tribo-filament is a refinement of the easy-to-machine igus iglidur I150 all-rounder filament. Because it is blue, it can be used to manufacture special parts that are optically detectable in the food industry. Food compatibility according to the FDA and to EU Regulation 10/2011 also qualifies the high-performance polymer for use in the food and cosmetics industries.

Read more...

FastConnect cable from igus reduces harnessing time by 46 per cent

Published on: April 22, 2021

igus now offers a new chainflex Profinet cable for fast cable harnessing in the field. For this purpose, igus relies on FastConnect technology, which ensures that the cable can be stripped easily in just a few steps. This allows assembly time to be reduced by 46 per cent. At the same time, the new Profinet cable has a long service life, especially in dynamic use in the energy chain, and a guarantee of up to 36 months.

Read more...

Advancing developments: igus honoured as SPE Network Pioneer Member

Published on: April 22, 2021

Single Pair Ethernet is currently one of the biggest trend topics in the field of data communication in order to be able to communicate with even the smallest sensors. In addition to compact connectors, slim cables are also in demand. For this purpose, igus has developed a highly flexible Single Pair Ethernet cable especially for dynamic use in the energy chain, and now also offers it harnessed as a ready-to-connect and tested readycable. To further advance the research of the technology, igus joined the SPE Industrial Partner Network in 2019 and has now received the “PIONEER Member” award.

Read more...