For highest precision and rigidity: new drylin linear bearings for shafts

Published on: May 13, 2021

In order to be able to move linear bearings on shafts with high precision, igus has now developed the W360CM series. The new polymer linear bearings consist of an aluminium housing and a thin liner, which ensure smooth and quiet operation combined with high rigidity. The bearings have hardly any clearance and allow precise movements. Thanks to the use of iglidur W360 high-performance polymers, the user does not need external lubrication. The dimensions of the new series match metallic ball bushings, so that they can be easily converted 1:1.

Read more...

Co-operation for recycling expanded: igus partner Mura Technology collaborates with Dow

Published on: May 13, 2021

The “Hydrothermal Plastic Recycling Solution” of startup Mura Technology promises the conversion of plastic back to oil in just 25 minutes. In order for entry into a sustainable circular economy to succeed, globally active industrial companies such as igus are supporting the development of this technology. Dow Chemical, the world’s second largest chemical company, is now another partner on board.

Read more...

igus 2021 Motion Plastics Show: 168 tribo innovations on the trade show stand

Published on: May 10, 2021

More new products, product extensions and digital offerings than ever before: the 2021 “igus Motion Plastics Show” is opening digitally. Visitors can look forward to 168 innovations from all departments – from telescopic robot tube packages to dry-running ball bearings with 21 times the standard service life to large scale 3D printing.

Read more...

Wound tribo plain bearings from igus reduce wear in heavy-duty applications

Published on: May 10, 2021

Especially for heavy-duty applications in the construction machinery or agricultural industry, igus now has the new tribo-material iglidur TX2 in its product range, which works without lubrication. Because even small excavators still need 50 litres of lubricant every year. The wound plain bearing bushings withstand very strong forces and increase wear resistance by a factor of 3.5 in load ranges with more than 100 MPa surface pressure.

Read more...

New triflex TRX energy supply system revolutionises 3D motion of robots

Published on: May 10, 2021

To ensure that cables on industrial robots can be guided in motion safely, easily and compactly, igus has now developed the four-dimensional triflex TRX energy chain. The new design study replaces classic robot hose packages and retraction systems. Special feature: 40 per cent retraction length ensured by a unique telescopic mechanism inside the chain. This allows users to save space on the third axis of their robot, up to 83 per cent weight and high costs for retraction systems.

Read more...