Custom-fit orthoses from the 3D printer

Published on: November 28, 2023

Produce orthoses that splint injured fingers in hospital in record time using a 3D printer: students at Trier University of Applied Sciences are developing a compact platform that measures fingers. The igus Young Engineers Support (yes) is supporting them by providing free miniature linear guides.

Read more...

Two drives in one: igus launches double-shaft stepper motor

Published on: November 23, 2023

Cost-effective automation in a confined installation space. To provide an easy introduction to automation, igus has now developed a new double-shaft stepper motor for its drylin linear technology. It can be used to drive two linear axes. Another possible application is the installation of a hand wheel on the second drive shaft. In an emergency, users can turn the motor by hand. Manual zero point calibration is also possible

Read more...

igus offers new record guarantee of four years on cables

Published on: November 23, 2023

If cables break, machines and systems come to a standstill. However, companies weren’t able to be sure how long a cable would last. Not until igus solved the problem: 10 years ago, igus was the first industrial company in the world to introduce a 36-month guarantee on moving cables. Just in time for the SPS 2023 automation trade fair, the plastics specialist is extending the guarantee period for its entire cable range by a further 12 months to four years. This gives customers even more functional and planning security. The guarantee, which is unique in the industry, is possible due to thousands of new customer applications and over 20 billion additional test cycles in the in-house chainflex laboratory carried out in the past decade.

Read more...

Position ready-to-install energy chains easily, quickly and accurately

Published on: November 21, 2023

If machines or systems are at a standstill, this costs production companies valuable time and money. To make it easier for customers to install energy supply systems and reduce installation time, igus offers the readychain service with pre-assembled systems consisting of chain, cables, connector and many other components. What makes it special: igus offers customers everything from a single source igus. The energy chain is filled, fully harnessed with connectors, quality-checked and delivered ready for connection – on request in the exact installation position. igus is now supplementing this service with a new “assembly helper”: the fast positioner. This simple tool makes handling ready-to-install e-chains even easier.

Read more...

Shaking hands with a robot: igus launches bionic hand for ReBeL cobot on the market

Published on: November 21, 2023

Robots have become an integral part of industry and are increasingly finding their way into small and medium-sized companies in the form of cobots, such as the ReBeL. They sort, pick and move with the help of cameras, suction devices and gripper systems. igus has now developed a finger gripper for the ReBeL cobot so that it can also perform humanoid tasks. It is made entirely of lubrication-free plastics, and is therefore very cost-effective and easy to integrate.

Read more...