igus develops first recyclable plastic bicycle frame

Published on: June 24, 2024

After RCYL, a bicycle made from 50 per cent recycled fishing nets, igus is setting the next milestone for sustainable mobility: the motion plastics specialist has developed the first bicycle frame made from recyclable plastic material for the German e-bike manufacturer Advanced Bikes, which is manufactured using injection moulding. Decades of expertise in plastics manufacturing and experience with the RCYL bike are channelled into the development of both the frame and new bicycle components made from high-performance plastics.

Read more...

iComm Box: all-in-one system for the next generation of condition monitoring

Published on: June 15, 2024

Optimise operating processes and minimise downtimes: this is what the new iComm Box from igus helps you with. Thanks to the communication module, the i.Sense sensors for condition monitoring of igus motion plastics can be seamlessly integrated into the superwise service. Intelligent algorithms provide a detailed status analysis of the monitored machines and systems. The superwise dashboard provides information in real time and allows for optimum monitoring and control. A decisive advantage: the costs for data transmission are already included in the product price.

Read more...

igutex plain bearing technology: belt and braces thanks to double winding

Published on: June 15, 2024

Handling containers around the clock under extreme conditions – this is the daily routine of STS, RMG and RTG cranes in ports around the world. However, premature wear and breakdowns of the wheel and axis units, the bogies, place an enormous burden on operators. In Rotterdam, igus will be presenting a solution at TOC Europe from 11th to 13th June 2024: wound, lubrication-free and corrosion-resistant polymer bearings from the igutex series for heavy-duty applications.

Read more...

igus develops first certified robotic energy supply system for dry cleanrooms

Published on: June 12, 2024

With the growing demand for electric cars, the need for high-quality lithium-ion batteries is also increasing. For this reason, they should ideally be manufactured in dry cleanrooms with minimal humidity and as little particulate matter as possible. At the same time, this environment must be automated because people are not allowed to spend long periods of time in dry cleanrooms. To ensure safe and reliable energy supply to robots, motion plastics specialist igus has developed the triflex R TRC: the first robot energy supply system with a certification for dry cleanrooms from Fraunhofer IPA for ISO Class 4-5.

Read more...

igus is adding live chat via WhatsApp to its customer service

Published on: May 12, 2024

The motion plastics specialist igus is now further expanding its customer service. Customer service employees can now also be reached via WhatsApp. Customers now have the option of conveniently using the igus live chat via the popular messaging platform to receive quick and uncomplicated support.

Read more...