Keyword:

Lubrication-free

New plastic bevel gears from igus for the lubrication-free drive around the corner

Published on: November 4, 2021

Bevel gears are suitable as drive elements in order to be able to transmit forces at a 90 degree angle. Especially for simple tasks, igus has now developed bevel gears made of two abrasion-resistant, durable high-performance plastics. They are not only lightweight and cost-effective, but also completely free of external lubrication. This reduces the time and cost of maintenance.

Read more...

Low-maintenance and durable: A flexible operating concept allows a clear view in construction machinery

Published on: September 29, 2021

Construction sites can be daunting, given all the machines, material and people. Keeping track of everything is difficult. A flexible new operating concept for driver’s cabs from Gessmann helps to ensure that operators always have the best possible overview of their surroundings. Because the tribo-plastics from igus used in the machinery require no lubricants or maintenance and therefore it remains relable over a long period of time.

Read more...

Horse 2.0: Electric all-rounder LyteHorse withstands desert, forest and water

Published on: September 14, 2021

The Canadian company LyteHorse Labs shows that electric vehicles do not perform poorly. The company has designed a new type of all-terrain electric vehicle that is suitable for a wide range of applications. On board are lubrication-free igus bearings that make the vehicle maintenance-free and corrosion-free, even in the most inhospitable environments.

Read more...

Completely relaxed gliding! Reliable motion of e-pedal boats through low-maintenance tribo-bearings from igus

Published on: October 6, 2020

Just relax on the lake or glide completely carefree through the lagoon, all this is made possible by the electrically assisted “Ceclo”. To ensure that the ride remains very smooth for a long time, the French manufacturer of the same name now installs polymer plain bearings from igus instead of metallic ball bearings in their e-pedal boats. As a result, the lubrication-free and maintenance-free rotation of the propeller reduces maintenance costs and also meets strict environmental regulations.

Read more...

Suitable for the desert! igubal pillow block bearings without lubrication align solar panels

Published on: September 10, 2020

To enable solar panels to generate energy efficiently, solar park operators rely on movable modules that automatically align themselves to the position of the sun and thus ensure a high energy yield. igus has developed the igubal ESQM pillow block bearing specifically for mounting the modules on square profiles and has now expanded it with two additional dimensions. Plant operators worldwide receive a lubrication-free solution, resistant to dust and dirt, whose durability has been tested in the laboratory and is guaranteed for 25 years.

Read more...

3D printing service from igus: worldwide delivery of lubrication-free components from 2 days

Published on: August 26, 2020

120,000 additively manufactured components were delivered by igus last year. Reason enough for the motion plastics specialist to further increase its capacities and equip its 3D printing service with new functions such as wall thickness and undercut analysis. In this way, customers worldwide can obtain their lubrication-free and low-maintenance components very easily and quickly, thereby saving costs.

Read more...

Fast and lubrication-free: new xiros film guide roller for labelling technology

Published on: July 24, 2020

They divert films or labels: guide rollers with ball bearings. Mainly used, so far, in clear anodised aluminium, the new black guide roller from igus now provides a real sensation in packaging and labelling technology. The ready-to-install system is convincing not only visually, but also technically. It consists of black anodised aluminium tubes and maintenance-free, smooth-running xiros polymer ball bearings.

Read more...

New igus SLS material for electrostatically conductive wear-resistant parts from the 3D printer

Published on: April 30, 2020

For safe and reliable production in the electronics and semiconductor industry, components are required that have electrostatically conductive properties. This is because even a small electric shock can destroy expensive production lines. igus has now developed a new stable material for the SLS method so that users can make their wearing parts with ESD properties flexibly and cost-effectively. The lubrication-free special parts made of iglidur I8-ESD can be printed and shipped within just few days.

Read more...

Maintenance according to the traffic light principle: smart drylin linear guide from igus

Published on: March 26, 2020

The drylin linear guide systems have to withstand extreme conditions in continuous operation or even in abrasive environments. In order to have the linear guides slide without lubricant, igus relies on linear bearings made of high-performance polymers. But when should I change the bearing? The new smart linear carriage from igus helps here. In accordance with the traffic light principle “stop when red, go when green”, the maintenance technician receives information about the maintenance requirement at the push of a button.

Read more...

Industry meets furniture technology: drylin linear rails for a sliding extension

Published on: March 17, 2020

Two pieces of furniture made by budding carpenters from Bergisch Gladbach demonstrates that industrial design combined with a Scandinavian look makes for unique furniture. Because they have that certain something extra, not only visually, but also functionally. This is ensured by lubrication-free drylin sliding linear guides – known by the industry. They allow smooth and maintenance-free movements in a bedside table with a linear guided element as well as in a coffee table with a pull-out unit.

Read more...