igutex TX3
In applications with loads of more than 80Mpa, plain bearings made of thermoplastic materials can be pushing their limits. igus has expanded the existing range of standard plain bearings with the new igutex fibre wound plain bearing series. The series displays its strength in heavy-duty areas such as construction machinery or hoists. The latest development in the product family is the material igutex TX3. It offers an even higher running performance with high dynamic forces than previous igutex bearings.