Reduce costs by up to 50% with the new miniature linear guide from igus

September 28, 2026

Compact drylin N linear system allows for adjustment tasks in the smallest of spaces and lowers assembly and maintenance effort

Compact, lightweight and lubrication-free: the new drylin N miniature guide from igus permits adjustment tasks in the smallest of spaces and reduces costs by up to 50% compared with similar recirculating ball bearing systems. (Source: igus SE & Co. KG)

More and more everyday objects are automated: from sample positioning in laboratories to fully automatic coffee machines to motorised extendable shelves and displays. Previously, many design engineers used miniature recirculating ball bearing systems for these adjustment tasks in very small spaces. The problem: the smaller the systems, the higher the manufacturing effort and, as a rule, the costs. igus is therefore launching a new miniature guide that permits cost savings of up to 50%. At the same time, the solution reduces the weight of applications as well as their assembly and maintenance effort.

The new miniature guide from the drylin N series consists of two components: an aluminium rail with a maximum length of 2,000 millimetres, which users can adapt to their application with millimetre precision, and a carriage made of lubrication-free high-performance plastic, on which superstructures can be mounted. The carriage slides directly on the rail and does not require any balls. “Thanks to this minimalist design and the choice of an extruded aluminium profile, the costs for the new miniature guide are up to 50% lower than those of conventional stainless-steel recirculating ball bearing systems,” explains Michael Hornung, Product Manager for drylin Linear and Drive technology at igus. “This enables design engineers to significantly reduce the costs of their linear guide, especially in applications with high quantities, without having to do without a compact and reliable guide solution.” The guide rails are available in silver or black anodised versions to reduce disturbing reflections in optical systems.

As light as a chocolate bar

The miniature guide is so compact that design engineers can also use it in particularly small and mobile applications, such as portable laboratory equipment. The aluminium rail is only 12 millimetres wide and 5 millimetres high. The carriages are available in two versions with lengths of 20 and 50 millimetres. Variable distances can be realised quickly and flexibly with short carriages. The long carriages, in contrast, are suitable for applications where only one carriage is to be used. “The solution is also particularly light,” says Hornung. “For example, a 500-millimetre-long rail and a 50-millimetre carriage together weigh only 45 grammes, about the same as a standard chocolate bar.” This benefits applications in the aerospace industry, for example, where every gramme saved reduces emissions. In robotics, for example in automated guided vehicles (AGVs), the solution can increase battery life due to its lower weight. Another advantage: the high-performance plastic used is free of PTFE and has been tested for the 96 PFAS compounds currently classified as particularly critical, which could be more strictly regulated in future.

Lubrication-free and suitable for glueing: assembly effort reduced by up to 80%

The drylin N miniature guide also reduces the effort involved in design, assembly and maintenance. igus already supports design engineers with digital services during the development phase. They can use online tools to calculate the expected service life of the linear guide quickly and easily. “This simplifies the design and shortens the time from the idea to high-volume production,” says Hornung. Assembly is also simple. “With recirculating ball bearing systems, assembly and precise alignment can cause additional effort,” says Hornung. “The drylin N guide rail is so light that it can even be glued instead of screwed, if necessary. We are currently conducting tests on this in our laboratory.” The carriages are available with a pre-tension so that they have no bearing clearance and run smoothly. In addition, the system is virtually maintenance-free thanks to its lubrication-free design. Microscopic solid lubricants are integrated into the high-performance plastic, ensuring low-friction dry operation without external lubricants.

Find out more about the new drylin N linear guide at:
drylin N NS-01-12 low-profile guide system | Miniature guide

Filename: PM4426-1.jpg

Filename: PM4426_EN.docx

Filename: PM4426_EN.pdf

Article keywords: