e-spool flex for continuous panel feed in industrial robots
January 21, 2021
ARAGON Industrieelektronik GmbH, a robotics service provider, uses a new slip ring-free igus cable unwinder

A control panel forms the robot’s control centre. If it is to be used flexibly, its cable must be not only several metres long, but also movable and safely stowed. To this end, igus has developed the e-spool flex. The new igus cable reel has no slip ring, so it can even supply bus signals with no interruptions. The cable can also be easily retrofitted into the system. These advantages won ARAGON over. It offers a complete cable set, consisting of e-spool flex with a standard cable and a pre-assembled panel mount, as a service for its industrial robots.
The task of ARAGON Industrieelektronik GmbH is to breathe new life into old robots. The leading industrial robotics provider offers global solutions for repairing, maintaining, retrofitting and tuning industrial robots. Some of its customers are relatively small companies that use up to ten robot systems. But larger companies and OEMs in the automotive industry also rely on ARAGON’s expertise. The company was looking for a practical cable solution specifically for use in control panels: “We are always trying to ensure our customers’ safety with innovative solutions. Until now, the cable was always on the floor, which made it easy to damage or trip over. So we went looking for a cable reel that had no interruptions and was quick and easy to retrofit”, says Iryna Geike, Global Country Manager at ARAGON. The company found what it was looking for in igus. “The new e-spool flex cable reel system was introduced to us and won us over immediately”, Geike recalls. The major advantages of the e-spool flex over other cable reels is that it does not use a slip ring. Media, data, and the power and signal supply for the emergency stop button can also be integrated into the system. Existing panel cables can simply be inserted into the system’s spiral guide and are automatically rolled up. “Our customers now receive a pre-assembled set consisting of the e-spool flex, ARAGON panel mount, cable, and a robot control cabinet mounting bracket for their control panels. The e-spool flex greatly extends the service life of the cable used and ensures more safety and order in the control panel”, Geike explains.
Rolling and unrolling cables: manually or automatically
igus offers the e-spool flex in several variants. One is a low-cost version with a manual turner or a cordless screwdriver to wind up the cable. Another is an automatic solution with a spring-driven return mechanism, a locking mechanism, and an optional retraction brake. ARAGON decided on the variant with the retaining spring. The cable roller is available in three sizes for cables with diameters of 5 to 15 millimetres and extension lengths of 5 to 15 metres. Cables can be replaced quickly at any time. In addition to subsequent integration of the e-spool flex into an existing cable system, igus offers the cable reel solution fully harnessed with chainflex cables specifically designed for moving applications. Cable durability in the e-spool flex is currently being extensively tested in the in-house 3,800 square metre igus test laboratory.