“RoHS” stands for “Restriction of Hazardous Substances” and regulates the use of hazardous substances in electronic devices. This EU directive aims to avoid harmful components such as lead, mercury or plasticisers in products and work environments. All of igus’ 1,354 highly flexible chainflex cables comply with the requirements of the current RoHS II directive. This ensures legal and functional safety for machine builders and safe use and disposal for the user.
De-icing and washing aircraft is still a very manual process. To reduce time, delays and therefore costs, MSG Production AS developed a fully automated all-in-one concept that can de-ice and wash aircraft. The Norwegian company relies entirely on the advantages of motion plastics from igus: energy chains of the E2 and E4 series ensure reliable cable guidance and igubal pillow block bearings for the mounting of cleaning nozzles.
Electromobility is a crucial topic of the future. For Germany to be in the pole position, it is important to inspire young minds to take up scientific and engineering professions. Towards this purpose, the annual JET Challenge takes place at the IdeenExpo in Hanover. Students are given the task of building a fast, tough and energy-efficient racing car from a standard, remote-controlled car with a limited budget. Wear-resistant 3D-printed gears from igus made from the high-performance plastic iglidur I6 helped in this endeavour.
CAT5e or CAT6 cables are indispensable for the implementation of Industry 4.0 in automation. igus has now further developed two highly flexible Ethernet cables, CFBUS.045 and CFBUS.049, specifically for use in the energy chain. The new CAT5e and CAT6 cables have enhanced UL approval for the North American market with 600 volts. They have been successfully tested in the igus test laboratory with more than 76 million strokes and are available from stock from a length of 1 metre.
Reduce costs by 40 percent, weight by 80 percent and save 100 percent lubricants. These are the advantages provided by igus plain bearings made of tribo-polymers, in contrast to metallic solutions such as DU, sintered or needle roller bearings. For all bearing points with standard dimensions, the customer can now rely on the new easy-to-use iglidur catalogue. With the help of a practical order code, the correct part number of standard materials can be easily found. A current price list provides information about the various differential prices.