Smart Factory with IoT: igus develops smart plastics app for Fanuc FIELD system

Published on: September 16, 2019

In order to be able to evaluate data from machines and systems centrally, Fanuc is now presenting its new open industrial IoT platform called “FIELD system”. The system can connect production machines of all manufacturers by means of a local network topology, enabling comprehensive data analysis of the entire process chain. In this infrastructure, apps from Fanuc and also from third-party suppliers are used. Now, igus has developed a smart plastics app for the new system. The app can be used by maintenance personnel to monitor the condition of their igus components, for example, energy chains and cables and plan all their maintenance work in good time.

Read more...

Openable igus energy chain for cleanrooms gets ISO Class 1

Published on: September 13, 2019

For a reliable energy supply in cleanrooms, igus has developed its modular and openable e-skin energy supply range. The energy chains provide plant with data, media and energy without unwanted particles contaminating the air. This was also proven by the Fraunhofer Institute IPA. All four energy chain types were convincing in the tests – with and without cables – and received the Fraunhofer Tested Device Certificate of ISO Class 1 for use in cleanrooms.

Read more...

igus 3D printing service: low wear plastic parts in 3 days!

Published on: September 10, 2019

Additive manufacturing gives designers new freedom and flexibility in the design of special solutions, including the development of efficient vehicle components. If lightweight and durable wear-resistant parts are required, igus offers the right solution from its 3D printing service. Users can order their special part made of tribologically optimised polymers from igus online in just a few seconds. You can choose from over 55 lubrication-free iglidur materials.

Read more...

Autonomous through the factory: this is how igus makes automated guided vehicles more fail-safe

Published on: September 4, 2019

In times of increasing digitalisation of factories and warehouses, au-tomated guided vehicles (AGVs) are continuously conquering intralo-gistics. The reliability requirements are high in order to ensure faster processing and unimpeded material flow. AGV manufacturers are therefore equipping their systems with motion plastics components from igus, which make the autonomous vehicles less maintenance-intensive, lighter and more energy-efficient.

Read more...

Backwards, forwards and in circles: igus provides fun on roller coasters

Published on: August 28, 2019

Sunshine, adrenaline, riding fun: more and more families are attracted to popular amusement parks, particularly in the summer months. Water rides are highly sought after especially when temperatures rise, including “Power Splash” from Mack Rides of Waldkirch. In order for the passengers to be able to get in and out safely, the developers of the water ride built a pivoting gate that placed special demands on the energy supply. igus provided the right solution with a rotary module.

Read more...