36-month guarantee on igus energy chains

Published on: February 18, 2020

Robust, lightweight and long-lasting: these are the qualities of the igus energy chains made from high-performance polymers. To ensure that users are always on the safe side, igus is now offering a 36-month guarantee on its energy chains. It is easy and quick for the customer to obtain the certificate. To do this, open the online service life calculator for e-chains and enter the dynamic specifications and the environmental conditions of the application. The online tool will then calculate the guaranteed service life of the energy chain. With one click, the customer receives the certificate by e-mail.

Read more...

Safety at high speed with the igus e-chain system in the linear motor robot

Published on: February 3, 2020

Twice as fast and half as heavy: this is what makes the linear motor robot from FIBRO LÄPPLE TECHNOLOGY (FLT) different from other solutions. In order for the linear robot to be able to get production up and running quickly and reliably, a compact, durable and quiet energy supply was required. A side-mounted igus energy chain system with pre-harnessed chainflex cables proved to be the optimal solution.

Read more...

When plastic becomes oil again: igus invests in chemical recycling pioneer

Published on: January 16, 2020

Renewable, sustainable and waste-reducing: these are the aims underpinning Cat-HTR (Catalytic Hydrothermal Reactor) technology. It can be used to recycle plastic waste within 20 minutes. The oil obtained can be used again to make new polymer products. In order to support the circular economy of plastics, igus has now invested €4.7 million in a company that plans to start up the first commercial Cat-HTR plant.

Read more...

Urmel’s lubrication-free return to the ice

Published on: January 10, 2020

Defrosting glaciers and declining fish stocks are just two examples of the effects of climate change in Alaska. In order to raise awareness of the issue among the population and to promote alternative drives, the Hoepner brothers from Berlin are developing their amphibious vehicle “Urmel”. They want to travel across Alaska with it. In order for Urmel to be able to drive over hill and dale and ice and snow, light and wear-resistant bearings are required. With the support of igus, the young inventors opted for lubrication-free iglidur tribo-polymers.

Read more...

The Best in Black: the new igus high-performance polymer iglidur J3B

Published on: January 10, 2020

For the bearing of pivoting and rotary applications, igus introduces iglidur J3, a lubrication-free and long-lasting tribo-polymer. The endurance runner convinces, above all, with its proven, very low coefficient of friction. As the yellowish material did not always match the design concept of the user, igus has now further developed the tried-and-tested tribo-polymer into the black iglidur J3B. But igus always has the right material for other applications as well. The intuitively operated iglidur online expert system helps with the selection.

Read more...