In semiconductor manufacturing, components such as energy chains and cables must meet the highest standards regarding their release of particles. In order to be able to develop new motion plastics that are suitable for use in cleanrooms, the Fraunhofer IPA, working as a development and certification partner on behalf of igus, has now designed and built a tailor-made cleanroom laboratory with an ISO Class 1 cleanroom system in Cologne. With the new lab, customer tests and the development of new products by the plastics specialist can be carried out in advance under realistic conditions in a very short time.
They divert films or labels: guide rollers with ball bearings. Mainly used, so far, in clear anodised aluminium, the new black guide roller from igus now provides a real sensation in packaging and labelling technology. The ready-to-install system is convincing not only visually, but also technically. It consists of black anodised aluminium tubes and maintenance-free, smooth-running xiros polymer ball bearings.
By increasing the voltage to 300V, users can now install the chainflex bus cables directly next to cables with a higher voltage level. Previously, all cables with different voltage classes had to be laid separately according to the specifications of the UL testing organisation. With the new, enhanced and UL-approved voltage class, the user optimises their technology and saves costs and time for the energy chain design.
Since the beginning of May, the igus innovations exhibition has been located in an exhibition hall in Cologne Porz-Lind. 100 motion plastics News are exhibited at the real igus trade show stand, and can be explored digitally either independently or together with igus experts. In June more than 18,000 visitors had already taken advantage of the unique offer and found out how they can improve the technology of their moving application and save costs with motion plastics.
High speeds, long travels and compact installation spaces: every two years, igus GmbH bestows the vector award, with which fascinating and creative energy chain applications are honoured. This year, 266 entries from 32 countries were received. The gold vector was won by the multi-spindle lathe of Gildemeister Italiana S.p.A.. In a very restricted installation space, a total of eight harnessed energy chains guide cables and hoses reliably and safely.