Evolution of the trapezoidal thread: new igus standard achieves 82 percent efficiency

Published on: March 15, 2022

Even tried and tested structures have potential for improvement. One example is the classic trapezoidal thread, which igus has refined. Thanks to a special geometric interaction between the lead screw nut, which requires no lubrication or maintenance, and the metal lead screw, dryspin technology promises a long service life, improved efficiencies, low wear and less movement noise. Now dryspin lead screw technology is available in eight new installation sizes.

Read more...

Supporting a new generation: igus is the top training company in 2022 – with its own trainee company

Published on: March 3, 2022

Cologne, 21th February 2022 – igus aims at further strengthening the company’s successful training model. In the “Germany’s Best Training Companies in 2022” study, the motion plastics specialist was awarded the third prize in the category rubber and plastics industry companies for its commitment to supporting young talent. But how does igus promote the next generation of skilled workers specifically? One answer: with their own trainee company.

Read more...

Low Cost Automation in XXL: large DIY palletiser from igus at a small price

Published on: February 15, 2022

The company igus is expanding its broad Low Cost Automation range with a new drylin XXL room linear robot. The linear robot has an action radius of 2,000 x 2,000 x 1,500 millimetres and is particularly suitable for palletising applications of up to 10 kilograms. The robot is available from 7,000 euros, including the control system, and is easy to set up and programme yourself using the do-it-yourself principle – without the help of a system integrator.

Read more...

Wear-resistant & lubrication-free: new igus bar stock for food, continuous operation and high media resistance

Published on: February 15, 2022

The company igus has expanded its wide range of iglidur round bars by no less than four materials; among them two for the food sector: the heat-resistant material iglidur AC500 and the resilient material A250. The extremely hard-wearing material iglidur H3 and the particularly wear-resistant endurance material iglidur E complete the product range. This makes it possible to mill and turn lubrication-free and maintenance-free prototypes and special components for a wide variety of applications.

Read more...

Lubrication-free rod ends: plastic-metal hybrid for higher loads in the food sector

Published on: February 7, 2022

Constant relubrication of metallic bearing points in the food industry costs time, money and increases the risk of contamination. Maintenance-free igubal spherical bearings from igus are an economical and safe alternative. Now, the motion plastics specialist is introducing a new model for higher loads. It is equipped with a stainless-steel housing, a self-lubricating polymer inner ring and a stainless-steel spherical ball. This allows for higher-load applications to be converted to future-proof tribo-technology.

Read more...