From recycling to bicycling: igus develops bicycle components for the mobility of tomorrow

Published on: June 22, 2023

After presenting the entirely plastic igus:bike last year, igus is now presenting an additional product line made of high-performance plastics for bicycle manufacturers. Other lines include frames made from a single mould or several components, impellers, and cranksets. The handlebars are about to go into series production and will be used on the Advanced Reco bike. The handlebars are produced with compounded polymers igus developed in house and have vigirously tested in the vast igus bicycle laboratory. The products are recyclable and made partly from recycled material. Production will start in Cologne and be expanded to Asia and North America, so as to offer bike OEMs local supply chains.

Read more...

Next-level recycling with digital innovations: Cologne-based plastics processor igus invests in start-up cirplus

Published on: June 15, 2023

Plastic products have many uses and have become indispensable for everyday life. But when they reach the end of their service life, they often end up in the incinerator. Conserving valuable resources and protecting the environment requires a sustainable plastics industry. The Cologne-based plastics specialist igus is pursuing this conservation goal with its “Chainge” recycling platform. The company has now invested in cirplus, a start-up based in Hamburg. The companies have a joint vision of closing the plastics cycle and initiating a revolution in the trade of recycled materials from technical and standard thermoplastics.

Read more...

University meets industry: developing innovative business models for the digital future together

Published on: June 5, 2023

The digital transformation in industry requires new business models for more flexible, efficient production. Technologies such as artificial intelligence and the internet of things are creating new opportunities to address customers with smart products and services. In the spirit of open innovation, igus, the motion plastics specialist, uses ideas from young talent to develop new solutions and has now participated in the first Hackathon by Innovation Hub Bergisches RheinLand e.V. As part of the project, TH Köln students developed concepts for use-based igus smart plastics business models.

Read more...

igus wins the “Going Circular” recycling competition held by the Cologne Chamber of Industry and Commerce

Published on: June 1, 2023

Rescuing plastics from incineration and integrating them into a circular economy: the unique “Chainge” program for recycling technical plastics won first place for igus in the “Going Circular” competition held by the Cologne Chamber of Industry and Commerce. The igus:bike, made entirely from recycled plastic, also made it to the finals.

Read more...

New igus xiros ball bearing materials stand up to chemicals and temperatures of 150°C

Published on: May 23, 2023

Things are heating up, especially in battery production for the automotive industry. Machines and systems have to withstand temperatures above 100°C and aggressive chemicals. For more machine reliability and less maintenance, igus has developed the lubrication-free xiros A500 deep groove ball bearing specifically for chemical and temperature resistance. To offer customers even more solutions, igus is adding two new materials to its range of ball bearings for high-temperature use. Users now also have access to the xirodur F500 cage material and balls made of zirconium oxide.

Read more...