80% lower CO2 footprint: igus switches to recycled material for energy chain series E2.1

April 16, 2025

Sustainable material igumid CG LW offers comparable mechanical specifications at the same price as the previous E2.1 series

For the entire E2.1 energy chain series, igus is switching to the recycled material igumid CG LW, further promoting the circular economy for plastics. (Source: igus GmbH)

Following the successful development of the world’s first energy chain made from recycled plastic, motion plastics specialist igus is taking the next step: the company is converting the entire catalogue range of its standard energy chain series E2.1 to the new recycled material igumid CG LW.

The European Union wants to establish a circular and climate-neutral economy by 2050 at the latest. Instead of producing waste, a functioning circular economy relies on the “cradle-to-cradle” concept. Consumables are returned to the natural and technical cycle so as to conserve valuable resources and raw materials. With the E2.1 energy chain series, which will be completely converted to recycled material this spring, igus shows that this is no longer a dream of the future. The company is taking this step after introducing the first energy chain made from recycled material in 2022. The energy chain series is now manufactured from the recycled material igumid CG LW. It consists of post-consumer recyclate, e.g. old fishing nets, and discarded energy chains, which are recycled and processed into recyclate as part of the in-house “Chainge” programme.

More sustainability without additional costs or loss of quality

The energy chains made from the sustainable material not only have mechanical specifications that are comparable to those of standard chains, but are also available at the same price as the previous E2.1 series. Even in terms of wear behaviour, stability and continuous flexing cycles, the energy chains offer the same quality. The series is characterised by a long service life, particularly quiet operation and easy filling and installation. “With this recycled chain series, we are enabling customers to make a contribution to the circular economy for plastics together with us,” says Jörg Ottersbach, Head of Business Unit e-chains at igus. “By switching to igumid CG LW, we are demonstrating that circular economy and cost-effectiveness are by no means mutually exclusive.”

80% lower CO2 footprint

By opting for the E2.1 series, customers are making an important contribution to the sustainable production of the future. Compared to the standard material, the recycled material has an 80% lower CO2 footprint. igus itself is also driving forward its sustainability measures with the new products. The company is focussing on measures in all areas (Scopes 1 to 3), from using process heat and green electricity to adding more e-charging stations to modernising buildings.

Around 170t of material collected

As part of the “Chainge” programme, igus has been taking back end-of-life energy chains from all manufacturers since 2019. In 2022, an online platform was added to the recycling initiative, through which customers can also recycle other components made of technical plastics while purchasing processed material in the form of regrind and regranulate. In addition to taking back old energy chains, igus also takes back old material as part of assembly orders. Around 170t of plastic have already been recycled via the “Chainge” platform. For its recycling programme, igus was awarded the Rhineland Business Prize in the sustainability category (2022) and took first place in the “Going Circular” recycling competition organised by the Cologne Chamber of Industry and Commerce (2023).

Filename: PM1425-1.jpg

Filename: PM1425-EN.docx

Filename: PM1425-EN.pdf

Article keywords: