When the robot monitors itself

Published on: November 27, 2025

Unplanned downtimes in automation not only cost time, but also money – especially in the automotive industry. With the new TR.P sensor, igus is launching a smart solution for industrial robots that actively monitors triflex energy chain systems and reacts immediately to critical tensile forces. The system recognises potential damage at an early stage, increases operational safety and provides support during commissioning through condition monitoring. igus will present the new solution at the SPS in Nuremberg (Hall 4, Stand 310).

Read more...

igus changes its legal form to SE & Co. KG and sets the course for further growth

Published on: November 25, 2025

igus GmbH, the specialist for motion plastics, has taken a significant step in its corporate development: the Cologne-based company is now trading under the name igus SE & Co. KG. With this new structure, igus is strengthening its strategic orientation, creating clear responsibilities and setting the course for future success – particularly with regard to international growth and corporate continuity. Artur Peplinski will assume the role of management spokesperson.

Read more...

Recognition for sustainable port solution: igus wins “Maritime Innovator of the Year” award

Published on: November 19, 2025

With its Mobile Shore Power Outlet (iMSPO), igus has developed a mobile shore power system for ports that can be moved flexibly depending on the position of the ships at the berth. The system allows ships to shut down their diesel engines in ports, switch to more environmentally friendly shore power and thus significantly reduce their CO2 emissions. For its central role in promoting sustainable and flexible port operations, igus has now been honoured as “Maritime Innovator of the Year”. The award was presented during the conference of the American Association of Port Authorities (AAPA) in Quebec, Canada.

Read more...

New PTFE-free 3D printing resin from igus with up to 122 times better wear rate

Published on: November 17, 2025

Just in time for Compamed, igus is launching a new resin for 3D printers that is PTFE-free and has been successfully tested for the 96 critical PFAS: iglidur i2000 is ideal for 3D printing of moving and friction-loaded components, such as gears in medical devices. Compared to standard resins, the new material has a wear rate that is up to 122 times better.

Read more...

More safety in cleanrooms with new polymer ball bearings from igus

Published on: November 11, 2025

In addition to energy chains, igus now also offers ball bearings made of abrasion-resistant high-performance plastics for cleanrooms. The new polymer bearings in the xiros series already fulfil the highest requirements of cleanroom production. They have been specifically developed for highly sensitive applications in battery production and the semiconductor industry, for example for use in conveyor rollers. The new ball bearings are characterised by very high resistance to abrasion and chemicals as well as minimised particle emissions.

Read more...

igus wins DLG Innovation Award for ReBeL cobot

Published on: November 11, 2025

Plastic specialist igus receives the prestigious Systems & Components Trophy – Engineers’ Choice Award from the German Agricultural Society (DLG). The ReBeL cobot – a compact, cost-efficient robot arm that sets new standards for automation in agriculture – won the award. In future, the robot will fulfil protection class IP67 so as to function reliably even under challenging environmental conditions.

Read more...

ReBeLMove Pro: modular robot platform for logistics, assembly and handling

Published on: November 2, 2025

Pressure in terms of costs and efficiency demands a lot from modern production. With the ReBeLMove Pro, igus is launching a modular autonomous mobile robot (AMR) that is easy to customise according to the modular principle – from small load carrier transport to robot solutions. It can be integrated into company processes without any previous experience. The ReBeLMove Pro is available from just €39,800, which makes it around 25 per cent more cost-effective than most competitor models.

Read more...