Plastic and heavy loads? This time igus proves that the combination works with a new lead screw nut design. The injection-moulded dryspin JGRM polymer nut offers a cost-effective alternative to ball screw nuts. The new lubrication-free and wear-resistant design can move heavy loads. For higher axial loads, the new lead screw nut is also available with a stainless steel plate as a “Heavy Duty version”.
The more than 70 submissions to the ROIBOT Award 2020 make it clear that entry into automation can be achieved easily and cost-effectively. This year, in addition to the expert jury, for the first time the public also has the chance to vote for their personal favourite. At www.roibot.de you can find many innovative examples of how Low Cost Automation from igus can be used profitably: from Bathroom mirror cabinet with sound system up to the automated “Chocomatic” praline dispenser.
To enable solar panels to generate energy efficiently, solar park operators rely on movable modules that automatically align themselves to the position of the sun and thus ensure a high energy yield. igus has developed the igubal ESQM pillow block bearing specifically for mounting the modules on square profiles and has now expanded it with two additional dimensions. Plant operators worldwide receive a lubrication-free solution, resistant to dust and dirt, whose durability has been tested in the laboratory and is guaranteed for 25 years.