Linear systems from igus as space-saving solution in award-winning furniture design

Published on: August 27, 2020

Living, working and cooking in confined spaces is currently part of everyday life for many people worldwide. This is why more and more practical furniture such as the multifunctional cube SQR is in demand. A square solution that combines kitchen, workplace and dining table. To create plenty of storage space, the inventor relied on the lubrication-free and long-lasting drylin linear guides from igus.

Read more...

Cables weighing tons guided by quickly mounted igus energy chain

Published on: August 26, 2020

It guides cables safely at a defined bend radius and even withstands shocks and impacts: the e-loop. The energy chain system is specifically designed for hanging applications, such as in deep drilling rigs and is already replacing service loops worldwide. In order to offer users a complete ready-to-connect system from a single source that operates safely even in extreme application scenarios, such as in explosion zones, igus now offers its energy chains with special connectors and cables as tested readychains.

Read more...

3D printing service from igus: worldwide delivery of lubrication-free components from 2 days

Published on: August 26, 2020

120,000 additively manufactured components were delivered by igus last year. Reason enough for the motion plastics specialist to further increase its capacities and equip its 3D printing service with new functions such as wall thickness and undercut analysis. In this way, customers worldwide can obtain their lubrication-free and low-maintenance components very easily and quickly, thereby saving costs.

Read more...

igus roller e-chain for targeted irrigation with savings potential

Published on: August 16, 2020

The aim of the precision irrigation carriage from Rathmakers Gartenbautechnik is to use water resources sensibly whilst protecting the groundwater at the same time. With the new automatic irrigation system, the water reaches exactly where it should: directly to the plants. For the safe and compact guidance of hoses and cables, the developers rely on an igus energy chain system consisting of roller chain and guide trough.

Read more...